Hello everyone;
I needed general information:
Can someone suggest me a dsp - board that has two Rj-45 onboard and work simultaneously.
Thank u
Please reply asap
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone;
I needed general information:
Can someone suggest me a dsp - board that has two Rj-45 onboard and work simultaneously.
Thank u
Please reply asap
The DM648 EVM has 2 ethernet jacks on it. That device has a 2 gigabit ethernet MACs and a 3-port switch integrated.
Thank you for ur help , can you please suggest me how do i find its technical reference because i cannot find it at ti.com
I been looking at C6455 ,but same problem cannot find its technical reference as well.
Thank you again for your timely reply
Amna
DM648 Product Folder
C6455 Support Home from Spectrum Digital
You can find Technical Reference Guides in the links above. Please note that the last time I checked it was not possible to run two separate instances of the NDK for each Ethernet port in the 3PSW. I will see if this is still the case.
thank you so much ; the links solved all my quires . But i couldnt find to much information about DM648 but it was helpful all da same .
In which board did this pb occured , i'll b looking forward .
i looking for a dsp board through which i can flow my Lan traffic and establish duplex communication between two stations . So is there any other board tht can be more useful plz suggest.
I also looked into C6452 DSP EVM , cant locate its technical document also ,it would b very kind of u if u can help me .
thank u
Amna
It looks like NDK v2.x introduced support for using both Ethernet ports on the DM648 3PSW.TimHarron said:Please note that the last time I checked it was not possible to run two separate instances of the NDK for each Ethernet port in the 3PSW. I will see if this is still the case.
We do not normally publish Technical Reference Manuals for a vendor's board on our website. While the DM648 TRM was published on our site, the C6452 EVM's is not. Please contact Lyrtech to see if they can make this available.Amna Rasul said:I also looked into C6452 DSP EVM , cant locate its technical document also ,it would b very kind of u if u can help me .
hello
i need 2 receive raw packet from lan n forward it to a pc . And this communication link has to be built through a dsp board.
so i need 2 rj45 connected to emac , working at da sametime NDK doesnt support raw frame option . So would Dm648 would b able to perform this task ?
and can 6452 evm perform this task as well ? has anyone worked on networking application using 6452 evm , please guide me ?
looking forward for reply
thank you
hello ;
Can u please tell me how DM648 support both ethernet ports. Can you please send me the code .
Can u kindly tell me , if i can capture raw ethernet frames on DM648 and if so how ?
Please reply soon
Thank u
Amna
Please download NDK 2.00 and read the documentation:
https://www-a.ti.com/downloads/sds_support/TargetContent/NDK/index.html