Part Number: TMS320C6455
My customer is looking to add the TMS320C6455BCTZ2, which is a 1.2GHz part as a substitute for TMS320C6455BCTZ. It appears that the 1.2G part should be a drop in replacement for the 1G part, without a need to change on-board clocks or PLL settings. Am I missing anything? I didn’t notice anything in the datasheet that said the parts couldn’t be run slower than their marked speed. I also didn’t see anything to suggest that the internal registers changed with speed grade.
Any assistance would be appreciated.