This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM6254 GPMC technology issue

Part Number: AM625

1. We search below description in datasheet, that the bootstrip pin isn't programmable via MUXMODE after the bootstrip is set to BOOTMODE, but we consider it is very waste because there are about 16pin bootstrip; 

   and we want to know that if we can set the bootstrip pin to other function for the MAXMODE( like the GPMC/ GPIO and so on);

2. We use the GPMC for the extend 16Bit SRAM for the FPGA communication, and now we want to konw how to identify the high and low 8 bits;

 \