This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet Raw Frame



Hello ;

Has anyone work on project relating to network on DSP , not related to NDK but actually worked at data link layer .

Kindly do answer , i can use ur guidance

thank u

  • For the most part I only see customers using the NDK when working with Ethernet on DSP only devices, even if not using the NDK in its entirety you may benefit from some of the lower level hardware abstraction layer (HAL) code so taking a look at the NDK may still help.

  • hello ;

    What if i dont assign any mac or ip to my dsp board , and pick all the frames on the network . Can tht be done if i use NDK ?

    Bec i read an article at wikipedia saying that NDK doesnt support ethernet raw frame because the memory uses increses really quickly in matter of seconds.

    Please tell me hal , b useful if i were to capture all the ethernet raw frame on network ?

    Regards

    Amna