This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I meet some error when I compile my project

Other Parts Discussed in Thread: CCSTUDIO

HI

    I  use ccs3.3,dm6467 demo

[Linking...] "C:\CCStudio_v3.3\tms470\cgtools\bin\cl470" -@"Debug.lkf"
<Linking>
>> warning: Cannot find state of callee routine at addr 0 called from module
            E:\Mr_deng\workbench\dsftest\ARM_Prog\DM6467EVM\DM6467_XGA_H264_ARM\Debug\ARM9_intvecs.obj

>>   error: relocation overflow occurred at address 0x00000000 in section
            '.intvecs' of input file
            'E:\Mr_deng\workbench\dsftest\ARM_Prog\DM6467EVM\DM6467_XGA_H264_ARM\Debug\ARM9_intvecs.obj'.  The 32-bit PC-relative displacement -536861899 at this location is too large to fit into the 24-bit PC-Relative field; the called function is out of range from this call site.  Consider using the '--trampolines' linker option to generate trampolines to bridge the distance between far caller/callee pairs.

>> warning: During relocation, cannot find state of routine at addr 0 called
            from module
            E:\Mr_deng\workbench\dsftest\ARM_Prog\DM6467EVM\DM6467_XGA_H264_ARM\Debug\ARM9_intvecs.obj

>>   error: relocation overflow occurred at address 0x00000008 in section
            '.intvecs' of input file
            'E:\Mr_deng\workbench\dsftest\ARM_Prog\DM6467EVM\DM6467_XGA_H264_ARM\Debug\ARM9_intvecs.obj'.  The 32-bit PC-relative displacement -536862769 at this location is too large to fit into the 24-bit PC-Relative field; the called function is out of range from this call site.  Consider using the '--trampolines' linker option to generate trampolines to bridge the distance between far caller/callee pairs.

>>   error: relocation overflow occurred at address 0x0000001c in section
            '.intvecs' of input file
            'E:\Mr_deng\workbench\dsftest\ARM_Prog\DM6467EVM\DM6467_XGA_H264_ARM\Debug\ARM9_intvecs.obj'.  The 32-bit PC-relative displacement -536869536 at this location is too large to fit into the 24-bit PC-Relative field; the called function is out of range from this call site.  Consider using the '--trampolines' linker option to generate trampolines to bridge the distance between far caller/callee pairs.