Part Number: AM3358
Other Parts Discussed in Thread: AM3359,
Hi.
In my project i used a AM3359 800MHz.
The MPU parameters are set at 600 MHz, and everything works fine.
Lunux boots everytime.
But due to the lack of AM3359 processors on market.
I was made to buy AM3358 1GHz.
I thought it will be replacement, but it is not.
Linux in the same configuration as previous (for AM3359) doesn't boot.
It starts to boot but fails to complete process.
Boot process stops at different moments, but always the same notice is sent.
[ 1.086339] Unable to handle kernel paging request at virtual address 73656369
[ 1.093598] pgd = 6afb7931
I don't have any idea how to solve problem.
Any help nice seen.
Marcin Gordel.
ZAZ-En sp. z o. o.