Part Number: TDA4VM
Hi Team,
I have a display with a resolution of 1440*900, but when I connected this display to display1 on tda4 through DP, the display showed "Input Not Supported".
Then, I replaced the display with another display with a resolution of 1920*1080. In this way, the output from tda4 could be displayed normally.
I would like to know how I can modify my code so that display1 of tda4 can transmit to my display (1440*900) normally?
In fact, my configuration is very simple, which is to directly use the interface provided by tiovx, specifically as follows:
In fact, I've been a little confused.
Judging from the interface provided by tiovx above, tiovx does not provide display adaptation. It seems the default target is 1920*1080.
I really have no idea how to modify this configuration. Could you please give me some advice?