I checked "12.6.2 Windowed Watchdog Timer (WWDT)" of TRM (Rev.A) and found some unclear points, so please answer the following unclear points.
1.
Does the read/write mode (User and privilege mode) in the description of the RTI_DWDCTRL Register indicate the "Arm Architecture" processor mode?
2.
The description of RTI_WDSTATUS[5]DWWD_ST in TRM states the following, but if the wrong key is written, RTI_WDSTATUS[2]KEYST will be "1" but RTI_WDSTATUS[5]DWWD_ST will remain "0" becomes.
"This bit denotes whether the timewindow defined by the windowed watchdog configuration has been violated, or if a wrong key or key sequence was written to service the watchdog."
Is this TRM description correct?