Part Number: PROCESSOR-SDK-DRA7X
hello,
I use XC5777X CPU BOARD to test ethernet.
The board has 2 ETH ports. I connect the 2 ports with ethernet cable.
why can't I get IP address of eth0 and eth1?
Thanks


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-DRA7X
hello,
I use XC5777X CPU BOARD to test ethernet.
The board has 2 ETH ports. I connect the 2 ports with ethernet cable.
why can't I get IP address of eth0 and eth1?
Thanks


Hi,
If you connect the board to a router or a PC that can provide IP address (DHCP), then they should automatically get the IP address.
Regards
Karthik
Hello Karthik:
Thanks for your reply
I connect a PC to the EVM eth1
the evm always prints "udhcpc: sending discover".
does it mean the PC has no ability to provide IP address(DHCP)?
what kind of PC can provide IP address?

hello Karthik:
I changed /etc/network/interfaces to static IP.
then I connect EVM eth1 and eth0 to my PC.
eth1 works, but eth0 fails.
do you know why eth0 fails?