Part Number: PROCESSOR-SDK-AM62X
Hi,
I am using AM62x-evm and default sdk.
I would like to test CAN on EVM either using shell script or anything. But I am not using CCS.
Is there any way to accomplish that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-AM62X
Hi,
I am using AM62x-evm and default sdk.
I would like to test CAN on EVM either using shell script or anything. But I am not using CCS.
Is there any way to accomplish that?
Hello Cyra,
Which CAN interface do you want to test, and which core do you want to use to control the CAN interface?
Regards,
Nick
Hi,
I would like to use pin 10 and 11 of J9; 16 and 22 of J9, connect those two pairs together and just test tx and rx.
Hello Cyra,
I assume you want to control MCU_MCAN0 and MCU_MCAN1 from the M4F core. I am reassigning your thread to a member of our MCU+ apps team.
Regards,
Nick
Cyra,
is there a specific reason you are not using CCS. please help us understand.
also have you tried running the MCAN examples described at links below
Regards
Anshu
We are just trying to develop a simple test application, preferably .sh format.
And setting up CCS seems quite complicated. I had tried it before and wasn't able to build.
But if CCS is the only way then i am willing to try again.
also have you tried running the MCAN examples described at links below
Won't it need CCS?
Cyra,
Thanks for the feedback on the complications involved in running CCS. can you help me understand what will be an ideal scenario for you in running the examples. which parts of running CCS is complicated for you. please feel free to send me an email. your feedback is very much appreciated. this will help us improve our offerings in order to serve our customers better in future.
Also if you want to understand which peripheral is supported and if you can control Main domain peripherals from MCU Domain please refer to Software Buildsheet here : https://software-dl.ti.com/mcu-plus-sdk/esd/AM62X/08_05_00_14/exports/docs/build_sheet/am62x-sw-buildsheet.html
Regards
Anshu
I will try again with CCS but in the mean time, is there any other way to do it without CCS?
Cyra,,
as mentioned in my previous post you can try working with makefiles. See the documentation here
there is also an option of using CCS Cloud, see more details here https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/08_04_00_17/exports/docs/api_guide_am64x/CCS_CLOUD_INTRO_PAGE.html
Please let me know if this helps. Also as mentioned earlier your feedback in using CCS will be very helpful
Regards
Anshu
cyra,
apologies for delayed response, please let me know the SDK you are trying to use, we have seen this kind of error before so be assured we will be able to help. I would also like to know the version of CCS being used
Regards
Anshu
Cyra,
can you try the FAQ here https://e2e.ti.com/support/processors-group/processors---internal/f/processors---internal-forum/1192328/faq-am62a7-import-sdk-examples-solving-the-am62ax-recognition-issue-in-ccs
This is shown for Windows but It should be same on Linux, we will try and update the FAQ on our end
Regards
Anshu
Hi Cyra,
Just to be clear and precise. You are trying to import the MCAN loopback polling example and facing a problem as stated in the screenshot.
You are also trying to import the example from MCU + SDK AM62x Version: 08.04.00.16 and you are doing this on Linux.
Please correct me if I missed anything else.
Regards,
Vaibhav
Hi Cyra,
I have found a fix.
Before you go over the link mentioned, I am going to simplify the fix in three simple steps:



After you have followed the above steps you should be good to go.
In case, you need further assistance feel free to let me know.
Alternatively, for your reference the link is: https://software-dl.ti.com/codegen/docs/tiarmclang/compiler_tools_user_guide/linux_installations.html
Thanks & Regards,
Vaibhav