Other Parts Discussed in Thread: INA231
Hi,
I am using am62x EVK.
I saw on another post that I can use ptool in order to read the value from INA23.
I used this command: sudo ./ptool -c configs/am62x_evm.conf -e
And got the following result.
This is the board.conf (am62x_evm.conf).
PM_BUS1 = { i2c = "1" VDD_CORE = { group = "CORE" address = "0x40" input = "VCC_CORE" output = "VDD_CORE" shunt_value = "0.002" shunt_accuracy = "1.0" } VDDR_CORE = { group = "CORE" address = "0x41" input = "VDD_0V85" output = "VDDR_CORE" shunt_value = "0.010" shunt_accuracy = "0.5" } SoC_DVDD3V3 = { group = "SOC_IO" address = "0x4C" input = "VCC_3V3_SYS" output = "SoC_DVDD3V3" shunt_value = "0.010" shunt_accuracy = "0.5" } SoC_DVDD1V8 = { group = "SOC_IO" address = "0x45" input = "VCC1V8" output = "SOC_DVDD1V8" shunt_value = "0.010" shunt_accuracy = "0.5" } VDDA_1V8 = { group = "ANALOG" address = "0x4D" input = "VDDA1V8" output = "VDDA_1V8" shunt_value = "0.010" shunt_accuracy = "0.5" } VDD_DDR4 = { group = "DDR" address = "0x47" input = "VCC1V2_DDR" output = "VDD_DDR4" shunt_value = "0.010" shunt_accuracy = "0.5" } }