Is DDR3 compatible with DDR2 or DDR (i.e. I can use DDR2 SDRAM to plug into the DDR3 interface):
a. in general,
b. for C6672?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is DDR3 compatible with DDR2 or DDR (i.e. I can use DDR2 SDRAM to plug into the DDR3 interface):
a. in general,
b. for C6672?
As mentioned DDR3 interfaces by default are not backwards compatible to DDR2. There are some devices which support both DDR3 and DDR2 through the same interface but most do not and Keystone (C66x) devices do not support DDR2 via the DDR3 interface.
Best Regards,
Chad