Part Number: AM625
Hello TI expert
I am optimizing the bootup timing for AM6254 board with ramdiskfs.
So, I saw the [ 10.216730] random: crng init done takes around 9 second
My config:
CONFIG_HW_RANDOM=y
CONFIG_HW_RANDOM_TIMERIOMEM=y
CONFIG_HW_RANDOM_OPTEE=y
How can I reduce this time to less than 1 second.
thanks,
Brian
[ 1.782240] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 1.789833] Freeing unused kernel memory: 8256K
[ 1.800813] Run /init as init process
[ 1.800821] with arguments:
[ 1.800823] /init
[ 1.800825] delayacct
[ 1.800828] with environment:
[ 1.800829] HOME=/
[ 1.800832] TERM=linux
[ 2.846882] random: dd: uninitialized urandom read (512 bytes read)
[ 2.976864] am65-cpsw-nuss 8000000.ethernet: down msc_sl e0000000 tmo 0
[ 2.998642] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 3.062663] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [NXP TJA1101] (irq=POLL)
[ 3.062699] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rmii link mode
[ 3.064567] MII_EXTSTAT=0x180;cable_report=0x0
[ 4.085523] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[ 10.216730] random: crng init done
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|