This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM: How to check whether the SBL has booted the MCU10_App?

Part Number: TDA4VM

Dear Expert,

      How could I check whether the SBL has loaded and booted the MCU10_App? My log is as follows and after Sciclient_procBootReleaseProcessor there was no further log. How could I check that the MCU10_App has been run correctly?

SBL Revision: 01.00.10.01 (Dec 30 2022 - 15:10:20)
SBL_ReadSysfwImage...gSciclient_firmware[0]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[1]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[2]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[3]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[4]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[5]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[6]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[7]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[8]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[9]=0x0
SBL_ReadSysfwImage...gSciclient_firmware[0]=0xc7038230
SBL_ReadSysfwImage...gSciclient_firmware[1]=0x30038230
SBL_ReadSysfwImage...gSciclient_firmware[2]=0x10203a0
SBL_ReadSysfwImage...gSciclient_firmware[3]=0x25140202
SBL_ReadSysfwImage...gSciclient_firmware[4]=0x43fb262d
SBL_ReadSysfwImage...gSciclient_firmware[5]=0x4dc0add8
SBL_ReadSysfwImage...gSciclient_firmware[6]=0x326ad708
SBL_ReadSysfwImage...gSciclient_firmware[7]=0x280cec31
SBL_ReadSysfwImage...gSciclient_firmware[8]=0x30a8c08e
SBL_ReadSysfwImage...gSciclient_firmware[9]=0x2a09060d
TIFS ver: 8.4.1--v08.04.01 (Jolly Jellyfi
SCISERVER Board Configuration header population... PASSED
Sciclient_setBoardConfigHeader... PASSED
Efuse xlated: VD 2 to 800 mV (OppVid: 0x37, Slave:0x48, Res:0x0)
Successfully set voltage to 800 mV for Slave:0x48, Res:0x0
Initlialzing PLLs ...done.
InitlialzingClocks ...done.
Initlialzing DDR ...Initlialzing DDR======== ...Board_DDRProbe: PASS
Board_DDRInitDrv: PASS
--->>> LPDDR4 Initialization is in progress ... <<<---
Reg Value: 128
Frequency Change type 1 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 0 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 1 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 0 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 1 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 2 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 1 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 2 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 1 request from Controller
Reg Value: 0
Reg Value: 128
Frequency Change type 2 request from Controller
--->>> Frequency Change request handshake is completed... <<<---
LPDDR4_Start: PASS
done.
Initializing GTC ...Begin parsing user application
SBL_BootImage>>>>>>>>>>>>>>>>>>>>>111111
SBL_RequestAllCores,>>>>>>>>>>>>>>>>>>>>>>>>> 0x16
Calling Sciclient_procBootRequestProcessor, ProcId 0x20...
Calling Sciclient_procBootRequestProcessor, ProcId 0x21...
Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
Calling Sciclient_procBootRequestProcessor, ProcId 0x2...
Calling Sciclient_procBootRequestProcessor, ProcId 0x6...
Calling Sciclient_procBootRequestProcessor, ProcId 0x7...
Calling Sciclient_procBootRequestProcessor, ProcId 0x8...
Calling Sciclient_procBootRequestProcessor, ProcId 0x9...
Calling Sciclient_procBootRequestProcessor, ProcId 0x3...
Calling Sciclient_procBootRequestProcessor, ProcId 0x4...
Calling Sciclient_procBootRequestProcessor, ProcId 0x30...
SBL_BootImage>>>>>>>>>>>>>>>>>>>>>22222222
SBL_OSPIBootImage>>>>>>>>>>>>>>>>>>>>>>>>>>>>>1111111
OSPI RCLK running at 166666666 MHz.
Ospi Read speed for 0x1c bytes from offset 0xc0000 = 0 Mbytes per sec
=======FSS_CTRL_REG_VALUE=[256]=========
Ospi Read speed for 0x1c bytes from offset 0xc0000 = 1 Mbytes per sec
Ospi Read speed for 0x1c bytes from offset 0xc1000 = 1 Mbytes per sec
Dias_SBL_select_system: abCfg as bellow:
ffffffffffffffffffffffffffffffffffffffffffffffffffffffff,crc=0d
ffffffffffffffffffffffffffffffffffffffffffffffffffffffff,crc=0d
Dias_SBL_select_system: boot from A system
SBL_MulticoreImageParse ImageOffset=0x300000
SSBL_VerifyMulticoreImage>>>>>>>>>>>>>>>>>>>>>>>>>1111
Ospi Read speed for 0x4 bytes from offset 0x300000 = 0 Mbytes per sec
SSBL_VerifyMulticoreImage>>>>>>>>>>>>>>>>>>>>>>>>>x509Header=0xc3068230
Searching for X509 certificate ...found @0x41c7fdc4, size = 1735 bytes
SBL reserved memory Found: Start = @ 0xb8000000, Size = 0x4000000
Copying 1736 bytes from app to 0xb8000001
Ospi Read speed for 0x6c8 bytes from offset 0x300000 = 16 Mbytes per sec
Found seq @ 0xb8000431
image length = 45232 bytes
Copying 45236 bytes from offset 0x3006c4 to 0xb80006c5...Ospi Read speed for 0xb0b4 bytes from offset 0x3006c4 = 20 Mbytes per sec
Cert @ 0xb8000001 ...Ignored on GP...done
SBL_RprcImageParse CoreId=0x1a
Detected lockstep for core_id 8, proc_id 0x1...
Calling Sciclient_procBootGetProcessorState, ProcId 0x1...
Sciclient_procBootSetProcessorCfg, ProcId 0x1, enabling Lockstep mode...
Calling Sciclient_procBootGetProcessorState, ProcId 0x1...
Enabling MCU TCMs after reset for core 8
Sciclient_procBootSetProcessorCfg update TCM enable/disable settings...
Copying 0x40 bytes to 0x0
Copying 0x1e0 bytes to 0x180
Copying 0x490 bytes to 0x41010c00
Copying 0x448 bytes to 0x41011090
Copying 0x318 bytes to 0x410114d8
Copying 0x118 bytes to 0x410117f0
Copying 0x4000 bytes to 0x41013f00
Copying 0x1800 bytes to 0x41ce2000
Copying 0x1400 bytes to 0x41ce3800
Copying 0x1400 bytes to 0x41ce4c00
Copying 0x1400 bytes to 0x41ce6000
Copying 0xb90 bytes to 0x70041200
Copying 0xc0 bytes to 0x70041e60
Setting Lockstep entry point for MCU1 @0x0
SBL_ospiClose called
SBL_ReleaseAllCores,>>>>>>>>>>>>>>>>>>>>>>>>> 0x16
Sciclient_procBootReleaseProcessor, ProcId 0x20...
Sciclient_procBootReleaseProcessor, ProcId 0x21...
Sciclient_procBootReleaseProcessor, ProcId 0x1...
Sciclient_procBootReleaseProcessor, ProcId 0x2...
Sciclient_procBootReleaseProcessor, ProcId 0x6...
Sciclient_procBootReleaseProcessor, ProcId 0x7...
Sciclient_procBootReleaseProcessor, ProcId 0x8...
Sciclient_procBootReleaseProcessor, ProcId 0x9...
Sciclient_procBootReleaseProcessor, ProcId 0x3...
Sciclient_procBootReleaseProcessor, ProcId 0x4...
Sciclient_procBootReleaseProcessor, ProcId 0x30...
Start SBL_SlaveCoreBoot >>>>>>>>>>>>>>>>11111
SBL_SlaveCoreBoot core_id=0x8, EntryPoint 0x0...
Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
Sciclient_procBootSetProcessorCfg, ProcId 0x1, EntryPoint 0x0...
Sciclient_pmSetModuleClkFreq, DevId 0xfa @ 1000000000Hz...
SBL_SlaveCoreBoot core_id=0x9, EntryPoint 0xffffffff...
Calling Sciclient_procBootRequestProcessor, ProcId 0x2...
Skipping Sciclient_procBootSetProcessorCfg for ProcId 0x2, EntryPoint 0xffffffff...
Sciclient_procBootReleaseProcessor, ProcId 0x2...
Sciclient_procBootReleaseProcessor, ProcId 0x1...