This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I created an SD card using the mksdboot.sh script in the [PSDK-LINUX-INSTALL-DIR]/bin in PSDK Linux 8.5. I do not see any interfaces corresponding to CPSW9G ethernet controller as well as no ethfw log. This issue occurs in J721e, J7200 and J784s4.
Hi,
From SDK 8.5 onwards the out-of-box configuration is changing. Hence, to enable the ethfw, you need to make some modifications for J721e (TDA4VM, DRA829), J7200 (DRA821) and J784s4 (TDA4VH)
This is a one-time setup.
SDK 8.5 :
Regards,
Tanmay