This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 usb_dev_serial example on linux

Trying to get the usb_dev_serial example to work under linux.  When usb cable is plugged in, I see the usb device and I see that it creates a /dev/ttyACM0 port.  I then write a simple C application to open this port and write/read to it.  I can write to it, and I get breakpoints while debugging the example code in the RxHandler method of Usb_dev_serial.c.  Problem is, the only event I ever get is USB_EVENT_DATA_REMAINING, so it never gets to any code which transmits anything back.

1) Am I treating this example properly (reading/writing to /dev/ttyACM0)?

2) Do I need to send special characters in order for this to work?

Any advice would be much appreciated.

Thanks, Dean