This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 Ethernet port tranformer

Hi.

Is it possible to remove the transformer from the ethernet port of dm6437 ??? I would like to connect with in 10 m range.

What will be the effect if the transformer is removed ???