Now i run run_app_tidl.sh on my board, i see some errors in logs.
I donot modify any tiovx code. So i want to known what is the matter. How to resolved it?
It is the logs in my board.
root@j7-evm:~# cd /opt/vision_apps/ root@j7-evm:/opt/vision_apps# root@j7-evm:/opt/vision_apps# ./run_app_tidl.sh APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 339.426593 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 339.437030 s: VX_ZONE_INIT:Enabled 339.437062 s: VX_ZONE_ERROR:Enabled 339.437073 s: VX_ZONE_WARNING:Enabled 339.437981 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! 339.438043 s: VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!! 339.786125 s: VX_ZONE_ERROR:[ownContextSendCmd:814] Command ack message returned failure cmd_status: -1 339.786154 s: VX_ZONE_ERROR:[ownContextSendCmd:850] tivxEventWait() failed. 339.786176 s: VX_ZONE_ERROR:[ownNodeKernelInit:538] Target kernel, TIVX_CMD_NODE_CREATE failed for node DisplayNode 339.786183 s: VX_ZONE_ERROR:[ownNodeKernelInit:539] Please be sure the target callbacks have been registered for this core 339.786189 s: VX_ZONE_ERROR:[ownNodeKernelInit:540] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel 339.786197 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.hwa.display ... failed !!! 339.786204 s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed 339.786211 s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed app_tidl: ERROR: Verifying display graph ... Failed !!! [MCU2_0] 339.785721 s: src/drv/disp/dss_dispApi.c @ Line 1856: [MCU2_0] 339.785774 s: Input width+startX/height+startY > display width/height [MCU2_0] 339.785863 s: src/drv/disp/dss_dispApi.c @ Line 1471: [MCU2_0] 339.785905 s: Set DSS parameter IOCTL failed [MCU2_0] 339.785954 s: VX_ZONE_ERROR:[tivxDisplayCreate:629] DISPLAY: ERROR: Display Set Parameters Failed! 339.787443 s: VX_ZONE_INIT:[tivxHostDeInitLocal:100] De-Initialization Done for HOST !!! 339.791830 s: VX_ZONE_INIT:[tivxDeInitLocal:193] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ... !!! DDR_SHARED_MEM: Alloc's: 15 alloc's of 26122863 bytes DDR_SHARED_MEM: Free's : 15 free's of 26122863 bytes DDR_SHARED_MEM: Open's : 0 allocs of 0 bytes DDR_SHARED_MEM: Total size: 536870912 bytes MEM: Deinit ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps#