This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GIO_submit hangon forever!



Hi,  I am working on C6748 UART using EDMA right now. I am using GIO_sunmit asynchronous call with a callback function. It works with Read. When I write to UART, I want to use Synchronous call with callbak function = NULL. But the GIO_submit call hongon there forever!

void

UART_RxCallback()

{

           SEM_post(&SEM_UART1_DataReady);

}

void

cUART::UART_init()

{

               EDMA3_DRV_Result edmaResult = 0;

 

              if (NULL == hEdma[0])

              {

                      edmaResult = edma3init();

                    if (edmaResult != EDMA3_DRV_SOK)

                   {

                                 /* Report EDMA Error */

                                LOG_printf(&trace,"\r\nEDMA3 : edma3init() failed\r\n");

                      }

 

            }

 

            Uart_init();

            uartParams = Uart_PARAMS;

            uartParams.hwiNumber = 9;

           uartParams.opMode = Uart_OpMode_DMAINTERRUPT;

          uartParams.rxThreshold = Uart_RxTrigLvl_1;

          uartParams.softTxFifoThreshold = 1;

 

          RxCAllbackFunction.fxn = (GIO_TappCallback)UART_RxCallback;

         RxCAllbackFunction.arg = NULL;

}

int

cUART::UART_GIO_Init(Void)

{

              GIO_Attrs gioAttrs = GIO_ATTRS;

             Int32 echoTskStatus = 0;

              Uart_ChanParams chanParams = {NULL};

             int status = 0;

 

            /* Initialize channel attributes. */

             gioAttrs.nPackets = 2;

            gioAttrs.timeout = SYS_FOREVER;

           chanParams.hEdma = hEdma[0];

            /* Initialize pinmux and evm related configurations */

           configureUart();

           /* Initialize UART Currently is been used to display a string */

          hUart_OUT = GIO_create("/UART0",IOM_OUTPUT,NULL,&chanParams,&gioAttrs);

          hUart_IN = GIO_create("/UART0",IOM_INPUT,&echoTskStatus,&chanParams,&gioAttrs);

          if ((NULL == hUart_IN) || (NULL == hUart_OUT))

         {

                    LOG_printf(&trace, "ERROR: Initialization of UART failed\n");

                  return 0;

           }

           //flush the Inout/Output buffer

           status = GIO_flush(hUart_IN);

           if(status != IOM_COMPLETED)

                    return 0;

            status = GIO_flush(hUart_OUT);

           if(status != IOM_COMPLETED)

                  return 0;

           return 1;

}

 

int

cUART::UART_Read(void * pData, int iLen)

{

              Ptr buf = NULL;

              Int status = 0;

              size_t len = iLen; //read one char everytime

 

             buf = Uart_RxBuffer;

              //use async read

              status = GIO_submit(hUart_IN,IOM_READ,buf,&len,&RxCAllbackFunction);

 

             //waiting for data read

             SEM_pend(&SEM_UART1_DataReady, SYS_FOREVER);

 

             memcpy(pData,buf,iLen);

             return status;

}

int

cUART::UART_Write(void *pData, int iLen)

{

             Ptr buf = NULL;

             Int status = 0;

            size_t len = iLen;

 

            //Copy to start string to Cache aligned buffer */

           memcpy(Uart_TxBuffer,pData,len);

 

           buf = Uart_TxBuffer;

 

           //use sync to write data

           status = GIO_submit(hUart_OUT,IOM_WRITE, buf, &len, NULL);

 

          if(!((status == IOM_COMPLETED)||(status == IOM_PENDING)))

          {

                     LOG_printf(&trace, "\r\n Error from GIO_write for UART\n");

           }

 

           return status;

}

I try to change the Write function using asynchronous way. But I allways get a IOM_PENDING return.

Could anyone help me out? Thanks, Yi