This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3354: Prevent Cursor appears in framebuffer display

Hi,

I am using the buildroot to compile the linux kernel 5.15.86.

And I found there is a cursor flashing on the LCD. So I want to prevent the cursor by disable framebuffer console.

But after me disable the configure:  CONFIG_FRAMEBUFFER_CONSOLE. The LCD can't work. Nothing display, except some White vertical line.

I'm following the guide: https://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components/Kernel/Kernel_Drivers/Display/LCDC.html

Using DRM framework:

And my DRM configure is 


#
# Graphics support
#
# CONFIG_IMX_IPUV3_CORE is not set
CONFIG_DRM=y
CONFIG_DRM_DP_AUX_BUS=y
# CONFIG_DRM_DP_AUX_CHARDEV is not set
# CONFIG_DRM_DEBUG_MM is not set
# CONFIG_DRM_DEBUG_SELFTEST is not set
CONFIG_DRM_KMS_HELPER=y
# CONFIG_DRM_DEBUG_DP_MST_TOPOLOGY_REFS is not set
CONFIG_DRM_FBDEV_EMULATION=y
CONFIG_DRM_FBDEV_OVERALLOC=100
# CONFIG_DRM_FBDEV_LEAK_PHYS_SMEM is not set
# CONFIG_DRM_LOAD_EDID_FIRMWARE is not set
# CONFIG_DRM_DP_CEC is not set
CONFIG_DRM_GEM_CMA_HELPER=y
CONFIG_DRM_KMS_CMA_HELPER=y

#
# I2C encoder or helper chips
#
# CONFIG_DRM_I2C_CH7006 is not set
# CONFIG_DRM_I2C_SIL164 is not set
# CONFIG_DRM_I2C_NXP_TDA998X is not set
# CONFIG_DRM_I2C_NXP_TDA9950 is not set
# end of I2C encoder or helper chips

#
# ARM devices
#
# CONFIG_DRM_HDLCD is not set
# CONFIG_DRM_MALI_DISPLAY is not set
# CONFIG_DRM_KOMEDA is not set
# end of ARM devices

# CONFIG_DRM_VGEM is not set
# CONFIG_DRM_VKMS is not set
# CONFIG_DRM_EXYNOS is not set
# CONFIG_DRM_UDL is not set
# CONFIG_DRM_ARMADA is not set
# CONFIG_DRM_RCAR_DW_HDMI is not set
# CONFIG_DRM_RCAR_LVDS is not set
# CONFIG_DRM_OMAP is not set
CONFIG_DRM_TILCDC=y
# CONFIG_DRM_VIRTIO_GPU is not set
# CONFIG_DRM_FSL_DCU is not set
# CONFIG_DRM_STM is not set
CONFIG_DRM_PANEL=y

#
# Display Panels
#

CONFIG_DRM_PANEL_SIMPLE=y

If I enable the CONFIG_FRAMEBUFFER_CONSOLE. The display work well.

If I disable the CONFIG_FRAMEBUFFER_CONSOLE, The display can't work.

I am hoping someone can suggest how I might track this down, and then hopefully disable it in the systemd startup scripts

Thanks for any suggestions.
Best regards,
Richard