This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6412: Producing a pinout (for symbol creation) for the AM6412 device.

Part Number: AM6412
Other Parts Discussed in Thread: SYSCONFIG,

Hello,

Which is the best route to produce a pin out , which will also include the Pin Muxing selection csv from the sysconfig tool ? Is it through the datasheet and sysconfig output ?

Example :

Using only the datasheet , the symbol would end up using the default function. If we want to use a different function , which will be selected through the sysconfig tool , should we use the output csv as well ?

Thanks

Alex