This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Error when executing ./vx_app_arm_remote_log.out

Genius 13655 points

Part Number: TDA4VM

Hello Champs,

HW: customer own board
SW:  0805 RTOS SDK

Customer tried to use 0805 RTOS SDK on his TDA4VM custom board, but it could not run well after executing ./vx_app_arm_remote_log.out

R core log shows as follows: 

[MCU2_0] 3747.906877 s: CIO: Init ... Done !!!
[MCU2_0] 3747.906952 s: ### CPU Frequency = 1000000000 Hz
[MCU2_0] 3747.906998 s: CPU is running FreeRTOS
[MCU2_0] 3747.907028 s: j721e APP: Init ... !!!
[MCU2_0] 3747.907057 s: SCICLIENT: Init ... !!!
[MCU2_0] 3747.907338 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[MCU2_0] 3747.907389 s: SCICLIENT: DMSC FW revision 0x15
[MCU2_0] 3747.907426 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0] 3747.907465 s: SCICLIENT: Init ... Done !!!
[MCU2_0] 3747.907494 s: UDMA: Init ... !!!
[MCU2_0] 3747.908932 s: UDMA: Init ... Done !!!
[MCU2_0] 3747.908994 s: MEM: Init ... !!!
[MCU2_0] 3747.909039 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!!
[MCU2_0] 3747.909122 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!!
[MCU2_0] 3747.909185 s: MEM: Init ... Done !!!
[MCU2_0] 3747.909214 s: IPC: Init ... !!!
[MCU2_0] 3747.909276 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_0] 3747.909327 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_0] 3759.282088 s: IPC: HLOS is ready !!!
[MCU2_0] 3759.297810 s: IPC: Init ... Done !!!
[MCU2_0] 3759.297880 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_1] 3747.823725 s: CIO: Init ... Done !!!
[MCU2_1] 3747.823796 s: ### CPU Frequency = 1000000000 Hz
[MCU2_1] 3747.823844 s: CPU is running FreeRTOS
[MCU2_1] 3747.823871 s: j721e APP: Init ... !!!
[MCU2_1] 3747.823897 s: SCICLIENT: Init ... !!!
[MCU2_1] 3747.824160 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[MCU2_1] 3747.824213 s: SCICLIENT: DMSC FW revision 0x15
[MCU2_1] 3747.824264 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_1] 3747.824303 s: SCICLIENT: Init ... Done !!!
[MCU2_1] 3747.824332 s: UDMA: Init ... !!!
[MCU2_1] 3747.826134 s: UDMA: Init ... Done !!!
[MCU2_1] 3747.826196 s: MEM: Init ... !!!
[MCU2_1] 3747.826240 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!!
[MCU2_1] 3747.826330 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!!
[MCU2_1] 3747.826391 s: MEM: Init ... Done !!!
[MCU2_1] 3747.826417 s: IPC: Init ... !!!
[MCU2_1] 3747.826478 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_1] 3747.826529 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_1] 3759.285868 s: IPC: HLOS is ready !!!
[MCU2_1] 3759.301598 s: IPC: Init ... Done !!!
[MCU2_1] 3759.301672 s: APP: Syncing with 5 CPUs ... !!!
[C6x_1 ] 3747.808001 s: CIO: Init ... Done !!!
[C6x_1 ] 3747.808032 s: ### CPU Frequency = 1350000000 Hz
[C6x_1 ] 3747.808043 s: CPU is running FreeRTOS
[C6x_1 ] 3747.808052 s: j721e APP: Init ... !!!
[C6x_1 ] 3747.808061 s: SCICLIENT: Init ... !!!
[C6x_1 ] 3747.808283 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C6x_1 ] 3747.808296 s: SCICLIENT: DMSC FW revision 0x15
[C6x_1 ] 3747.808306 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_1 ] 3747.808316 s: SCICLIENT: Init ... Done !!!
[C6x_1 ] 3747.808326 s: UDMA: Init ... !!!
[C6x_1 ] 3747.810048 s: UDMA: Init ... Done !!!
[C6x_1 ] 3747.810071 s: MEM: Init ... !!!
[C6x_1 ] 3747.810086 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ dc000000 of size 16777216 bytes !!!
[C6x_1 ] 3747.810104 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_1 ] 3747.810120 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ dd000000 of size 50331648 bytes !!!
[C6x_1 ] 3747.810137 s: MEM: Init ... Done !!!
[C6x_1 ] 3747.810146 s: IPC: Init ... !!!
[C6x_1 ] 3747.810169 s: IPC: 6 CPUs participating in IPC !!!
[C6x_1 ] 3747.810185 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_1 ] 3759.271686 s: IPC: HLOS is ready !!!
[C6x_1 ] 3759.275887 s: IPC: Init ... Done !!!
[C6x_1 ] 3759.275915 s: APP: Syncing with 5 CPUs ... !!!
[C6x_2 ] 3747.823550 s: CIO: Init ... Done !!!
[C6x_2 ] 3747.823579 s: ### CPU Frequency = 1350000000 Hz
[C6x_2 ] 3747.823590 s: CPU is running FreeRTOS
[C6x_2 ] 3747.823599 s: j721e APP: Init ... !!!
[C6x_2 ] 3747.823608 s: SCICLIENT: Init ... !!!
[C6x_2 ] 3747.823831 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C6x_2 ] 3747.823843 s: SCICLIENT: DMSC FW revision 0x15
[C6x_2 ] 3747.823854 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_2 ] 3747.823865 s: SCICLIENT: Init ... Done !!!
[C6x_2 ] 3747.823875 s: UDMA: Init ... !!!
[C6x_2 ] 3747.825813 s: UDMA: Init ... Done !!!
[C6x_2 ] 3747.825834 s: MEM: Init ... !!!
[C6x_2 ] 3747.825849 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ e0000000 of size 16777216 bytes !!!
[C6x_2 ] 3747.825867 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_2 ] 3747.825883 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e1000000 of size 50331648 bytes !!!
[C6x_2 ] 3747.825900 s: MEM: Init ... Done !!!
[C6x_2 ] 3747.825909 s: IPC: Init ... !!!
[C6x_2 ] 3747.825930 s: IPC: 6 CPUs participating in IPC !!!
[C6x_2 ] 3747.825945 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_2 ] 3759.275825 s: IPC: HLOS is ready !!!
[C6x_2 ] 3759.279731 s: IPC: Init ... Done !!!
[C6x_2 ] 3759.279761 s: APP: Syncing with 5 CPUs ... !!!
[C7x_1 ] 3747.900459 s: CIO: Init ... Done !!!
[C7x_1 ] 3747.900475 s: ### CPU Frequency = 1000000000 Hz
[C7x_1 ] 3747.900488 s: CPU is running FreeRTOS
[C7x_1 ] 3747.900496 s: j721e APP: Init ... !!!
[C7x_1 ] 3747.900505 s: SCICLIENT: Init ... !!!
[C7x_1 ] 3747.900743 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C7x_1 ] 3747.900760 s: SCICLIENT: DMSC FW revision 0x15
[C7x_1 ] 3747.900771 s: SCICLIENT: DMSC FW ABI revision 3.1
[C7x_1 ] 3747.900783 s: SCICLIENT: Init ... Done !!!
[C7x_1 ] 3747.900793 s: UDMA: Init ... !!!
[C7x_1 ] 3747.902190 s: UDMA: Init ... Done !!!
[C7x_1 ] 3747.902206 s: MEM: Init ... !!!
[C7x_1 ] 3747.902219 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 117000000 of size 268435456 bytes !!!
[C7x_1 ] 3747.902242 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!!
[C7x_1 ] 3747.902260 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!!
[C7x_1 ] 3747.902286 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!!
[C7x_1 ] 3747.902304 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ 100000000 of size 385875968 bytes !!!
[C7x_1 ] 3747.902324 s: MEM: Init ... Done !!!
[C7x_1 ] 3747.902333 s: IPC: Init ... !!!
[C7x_1 ] 3747.902350 s: IPC: 6 CPUs participating in IPC !!!
[C7x_1 ] 3747.902367 s: IPC: Waiting for HLOS to be ready ... !!!

what about this issue? 


Thanks
Regards
Shine