Other Parts Discussed in Thread: TMS320DM6437
Hi all
I can't read GP[1] on my TMS320DM6437. The pin is set up as an input (GPIO_DIR01 = 0xFFFFFFFF), and I'm pretty sure the pin multiplexing is set up right also. We're booting without PCI enabled (PCIEN pin is wired to ground, and the bootmode configuration register confirms this reading 0x00104104). GP[0] can be read without problems.
Anthony Berthet from the European support centre suggested I recheck my PINMUX settings for violations on the reserved bits (this caused a problem in this case) but I'm sure this is not the issue on my settings(CFG_PINMUX0 = 0x00140101; CFG_PINMUX1 = 0x01004140).
I have this problem across multible PCBs, all of which are working perfectly fine otherwise.
Does anyone have any suggestions?
Thanks
Leon de Wit