I just recieved a DM37x eval board I am having issues with it. And I don’t want to make any changes to the SD card. And can’t seem to make a working copy of it. I bought an 8 gig SD card, it won’t boot. I get this message:
Texas Instruments X-Loader 1.46 (Mar 24 2011 - 20:21:25)
ONENAND Flash Unsupported
OneNAND Unsupported !
X-Loader hangs
Is there a special kind of SD card I need to get to make a bootable copy? If so what kind? I can’t read what kind came with the board, because of the labels.
I have tried just putting the uboot partition on a 2 gig SD card, and it won’t even try to boot. What am I doing wrong?
Also the TI SD card gets lots if errors on boot up during uboot. Is this normal?
U-Boot 2009.11 (Mar 24 2011 - 20:27:06)
AM37x/DM37x-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 EVM board + LPDDR/NAND
I2C: ready
DRAM: 256 MB
NAND: 512 MiB
err_loc=2509
err_loc=-1144
err_loc=-1311
err_loc=-2375
err_loc=3924
err_loc=3686
err_loc=959
err_loc=-3521
err_loc=3535
err_loc=2218
err_loc=-1854
err_loc=-1959
err_loc=1141
err_loc=559
err_loc=-860
err_loc=-2114