We are migrating the Linux-BSP on one of our projects from 4.19 to 5.10
In doing so we got few compilation errors on DTS and we had to update the DTS for few of the nodes.
Attached is what we did to get it compiled and compatible with Linux-5.10
I need to ascertain if these changes are inline with what was originally happening w.r.t DTS on 4.19.
Attaching image for reference
Would appreciate some help here
Thanks
-maheshG