Is it possible to connect the AM3517 as a slave device to the MSP430? If so, how? UART? Also, what would be the software implications if any.
We have a lot of code effort invested in the MSP430 and we want the AM3517 as a QVGA LCD driver to the MSP430. Yes, we understand that it is better to just port the entire design over to the AM3517, but we are looking at our options to use our existing validated hardware and software.