This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

evmc6472 and execution functions in parallel range



Hello

I'm using the CCSv4.2 , BIOS5 and evmc6472 platform.

I want to run two functions in parallel range, the first function is running on the core0 and the  second in the others cores, and then re-use the results of these two functions to compute another variable.

/**********************************************************************************************************************/

void main( )

{

CoreNum = CSL_chipReadReg( CSL_CHIP_DNUM );

for(j=0;j<size;j++)
    {
        buf1[j]=2*j;
        buf2[j]=4*j;
    }
    if ( CoreNum == 0 )
    {
        sum0=sum(buf1,buf2); // compute the sum of each coeff of *buf1 with *buf2
        printf("the sum  = %d  \n",sum0); 
    }
    else
    {
        prod0=Prod(buf1,buf2); // compute the sum of multiplying each coeff of *buf1 with *buf2
        printf("the result  = %d  \n",prod0);
    }

div=(float)prod0/sum0;

printf("result of the division = %f \n",div);

}

/****************************************************************************************************************/

the problem is that the result of the division  "div"  is not correct because I think that the two functions have not the same time of execution.so the core compute the div 

while the core 1 doesn't terminate the computing of prod0. so could you tell me what command I have to add in the code to compute the div when the result sum0 and prod0 are ready both.

Please can you tell me how can I verify that the two function are executed in parallel...I tried by using the CPU Load graph but I didn't see any think.

I will be very thankfull..

Cordialy

David