This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1707 DevKit from spectrum digital. Who can give me an SD-card image for this board ?

Other Parts Discussed in Thread: AM1707, OMAP-L137

Sorry for my English and for my dumb questions (I am a novice in Linux).

The original SD Card was broken. Tell me please, where can I download an image. Or maybe I can to create this image myself ? As I can undertand, SD-card contains the Rootfs. Thats why Linux tell me "Kernel Panic":

 

Booting U-Boot:

U-Boot > printenv
bootargs=mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p1 rw rootwait ip=off

Booting Linux:

omap_rtc omap_rtc: setting system clock to 2000-01-06 17:17:35 UTC (947179055)
Waiting for root device /dev/mmcblk0p1...
mmc0: new high speed SD card at address 0002
mmcblk0: mmc0:0002       1.88 GiB
 mmcblk0: unknown partition table
VFS: Cannot open root device "mmcblk0p1" or unknown-block(179,1)
Please append a correct "root=" boot option; here are the available partitions:
1f00             256 mtdblock0 (driver?)
1f01              16 mtdblock1 (driver?)
1f02            3824 mtdblock2 (driver?)
b300         1974272 mmcblk0 driver: mmcblk
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,1)
Backtrace:
[<c002f718>] (dump_backtrace+0x0/0x114) from [<c02f32f4>] (dump_stack+0x18/0x1c)
 r7:00008000 r6:c1c11000 r5:c0024a08 r4:c0403ab8
[<c02f32dc>] (dump_stack+0x0/0x1c) from [<c02f335c>] (panic+0x64/0x13c)
[<c02f32f8>] (panic+0x0/0x13c) from [<c0008fec>] (mount_block_root+0x1e0/0x220)
 r3:00000000 r2:00000001 r1:c1c23f60 r0:c037ebf6
[<c0008e0c>] (mount_block_root+0x0/0x220) from [<c00090f0>] (mount_root+0xc4/0xfc)
 r8:00000000 r7:00000000 r6:00000000 r5:c0024a08 r4:0b300001
[<c000902c>] (mount_root+0x0/0xfc) from [<c0009298>] (prepare_namespace+0x170/0x1c8)
 r5:c0024a08 r4:c04035c0
[<c0009128>] (prepare_namespace+0x0/0x1c8) from [<c00084c8>] (kernel_init+0xf0/0x12c)
 r5:00000000 r4:c0403380
[<c00083d8>] (kernel_init+0x0/0x12c) from [<c0042768>] (do_exit+0x0/0x6b4)
 r5:00000000 r4:00000000

 

  • The TI Wiki has a lot of pages on the OMAP-L137 which is more or less that same as the AM1707. See here for SD Card

    http://processors.wiki.ti.com/index.php/Creating_filesystems_on_removable_media

    A single parition EXT2 parition FS should work. The actual filesystem tarball will be buried in on the many packages on the DVDs that cam with the kit. I forget exactly where.  Well...I got disks with my OMAP-L137 EVM. You can probably download the from the AM1707 product website

    http://focus.ti.com/docs/prod/folders/print/am1707.html
    http://focus.ti.com/docs/toolsw/folders/print/linuxsdk-am1x.html
    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/sdk/AM1x/1_10/latest/index_FDS.html