Hello everybody.
Now I'm using DM365 and I have used the NAND(samsung K9F1G08UC) but it has been kill off the produce.
so I decided to change the nand part to K9F1G08U0D–SCB0 .
However, we are currently facing serious problems.
current symptoms is that Nand writing is no problem. all files - UBL,Bootloader, kernel, ramdisk - writing without error.
After reboot, UBL and u-boot works fine.
But, when I read the Nand section on the u-boot prompt, every Nand section are recognized bad section include ubl, u-boot and can't read the data.
I have no idea what's going on.
When I compare to both datasheet, read/write timing is a bit changed and ECC detection is changed from 4bit to 1bit.
Current nand write use 4bit ECC. if it's changed, does it possible to occurs above error?
I searched the e2e, but it seems no problem.( http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/98648/345060.aspx#345060 )
What do I need to check?
We should go into mass production right now. Please give a goot hint.
Regards.
Jay.