Hello
Is anyone knows if activating GDR function at this platform (365) has any limitations ?
I mean when working at bits/slice mode it should work fine ? or it works only with MB/Slice mode ?
When activating GDR both with Enable_GDR=1 & Enable_GDR=2, the image is courrpted and there are
image artifacts .After few minutes the image is freezing totaly .
Other issue Multiple slice = ON has affects too ?
Regards
Gidi