About the power rail of
VDD_CORE(0.75V) and VDDA_CORE_USB(0.85V) is different ,but in the notes 2 mentioned the difference between VDD_CORE and VDDA_CORE_USB should be within+/-1%.
Which seems conflict with each other.
BR Jingcheng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About the power rail of
VDD_CORE(0.75V) and VDDA_CORE_USB(0.85V) is different ,but in the notes 2 mentioned the difference between VDD_CORE and VDDA_CORE_USB should be within+/-1%.
Which seems conflict with each other.
BR Jingcheng
Hello Jingcheng ye,
Thank you for the query.
Two operating voltages are supported for VDD_CORE, VDDA_CORE_CSIRX0, VDDA_CORE_USB, VDDA_DDR_PLL0. Use of 0.75V or 0.85V provides design flexibility to designers.
Regards,
Lavanya M R.