Part Number: TMDX654GPEVM
I have looked at the users guides for the TMDX654GPEVM & TMDX654IDKEVM. It is not clear if the boards provide external access to all three PRUs. The application connector shows GPIO pins connected to PRU0 and PRU1. I need to access all three for external connections to a a set of ADC chips. A dual core PRU is required to acquire and move data to main memory for each chip, as well as an additional PRU core to control the 3 wire SPI interface to the chips. I have implemented a single channel system on a Beagle Bone AI AM5729 and need to scale this up for the AM65xx.
Bottom Line; Does the TMDX654 GP or IDK allow direct access to all three PRUs via pinmux config or other means for external input?