Other Parts Discussed in Thread: SYSCONFIG
Hello everybody,
we would like to evaluate the option of using the GPMC in 32-bit wide A/D non-multiplexed mode.
Document SPRUIM2E (9/2022, page 7417)
....
• External ... 32-bit pseudo-SRAM (pSRAM) device
....
seems to indicate that this is an option.
Table 12-3453, contains the pin-outs for
...
- non-multiplexed Address Data 16-Bit Device
- non-multiplexed Address Data 8-Bit Device
...
but not for non-multiplexed Address Data 32-bit Device.
Is it save to assume that in a 32-bit configuration GPMC0_AD[31] .. GPMC0_AD[16] would act as data bits 31..16?
If so is it possible to add that to the manual?
If this mode will not work please -please correct me and also remove confusing hints from the tech specs.
Thanks for your help -
FW