This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L138 OMAP issue

Hi,

I have got a Zoom OMAP L138 EVM board which includes an LCD interface also. Currently I am trying to display the output of a program on the LCD screen. I have two concerns here:

 

1)      The over-all speed of the program is very slow. Is it because Iam running in debug mode? The GEL file initialization is as follows:

C674X_0: Output: Target Connected.

C674X_0: Output: ---------------------------------------------

C674X_0: Output: Memory Map Cleared.

C674X_0: Output: ---------------------------------------------

C674X_0: Output: Memory Map Setup Complete.

C674X_0: Output: ---------------------------------------------

C674X_0: Output: KICK Unlocked.

C674X_0: Output: ---------------------------------------------

C674X_0: Output: PSC0 Enable Verify Timeout on Domain 0, LPSC 6

C674X_0: Output: PSC Enable Complete.

C674X_0: Output: ---------------------------------------------

C674X_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz

C674X_0: Output: mDDR initialization is in progress....

C674X_0: Output: PLL1 init done for DDR:150MHz

C674X_0: Output: Using mDDR settings

C674X_0: Output: mDDR init for 150 MHz is done

C674X_0: Output: ---------------------------------------------

C674X_0: Output: DSP Wake Complete.

C674X_0: Output: ---------------------------------------------

 

2)      The programmed LCD width is only 480, and I need to display atleast 2500 samples at one frame? How can I tackle this issue? Can you guide to some link which talks about LCD interface. I am able to display for 480 samples.

 

Thanks and regards,

 

Mahesh