Part Number: TMDSIDK572
I have the board "TMDSIDK572 EVM".
With the help of the PROCESSOR-SDK-LINUX-AM57X (Version 08_02_01_00) I want to build the image "tisdk-default-image".
I have performed all the steps described in the section "Download and Install the SDK" (software-dl.ti.com/.../Download_and_Install_the_SDK.html).
In the section "Building the SDK" (file:///home/stranzjm/Projects/ti-am57x/PROCESSOR-SDK-LINUX-AM57X/ti-processor-sdk-linux-08_02_01_00/docs/linux/Overview_Building_the_SDK.html) is described how to build the image "tisdk-default-image".
Regarding the cross-compile toolchain, it only says: "Download the toolchain compilers from the links provided in the SDK release page."
However, I did not find a link to it!
If you start the build process with
MACHINE=am57xx-evm bitbake tisdk-default-image
then it reports that the no toochain "gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf" was found.
I then downloaded the toolchain "gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz" from the website "">developer.arm.com/.../gnu-a" and unpacked it.
The build process was then restarted with
TOOLCHAIN_BASE=~/Projects/ti-am57x/PROCESSOR-SDK-LINUX-AM57X/toolchain MACHINE=am57xx-evm bitbake tisdk-default-image
Unfortunately the build process is aborted after some time in an error in the recipe "linux-ti-staging_5.10.bb"; the error messages are in the attached file "build_error.txt".
What should I do?
Is there a suitable download link for "ti-processor-sdk-linux-08_02_01_00" for the toolchain to be used?
Jan-Marc.
ERROR: linux-ti-staging-5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14 do_compile: oe_runmake failed ERROR: linux-ti-staging-5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14 do_compile: Execution of '/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/temp/run.do_compile.3704' failed with exit code 1 ERROR: Logfile of failure stored in: /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/temp/log.do_compile.3704 Log data follows: | DEBUG: Executing shell function do_compile | NOTE: make -j 6 HOSTCC=gcc -isystem/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/include -O2 -pipe -L/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -L/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,-rpath,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E HOSTCXX=g++ -isystem/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/include -O2 -pipe -L/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -L/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,-rpath,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native/lib -Wl,-O1 uImage CC=arm-none-linux-gnueabihf-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14=/usr/src/debug/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14 -fdebug-prefix-map=/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14=/usr/src/debug/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14 -fdebug-prefix-map=/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot= -fdebug-prefix-map=/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/recipe-sysroot-native= -fdebug-prefix-map=/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source=/usr/src/kernel LD=arm-none-linux-gnueabihf-ld.bfd LOADADDR=0x80008000 DTC_FLAGS=-@ | GEN Makefile | HOSTCXX scripts/gcc-plugins/arm_ssp_per_task_plugin.so | HOSTCC scripts/extract-cert | In file included from /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/scripts/gcc-plugins/gcc-common.h:139:0, | from /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/scripts/gcc-plugins/arm_ssp_per_task_plugin.c:3: | /home/stranzjm/Projekte/ti-am57x/PROCESSOR-SDK-LINUX-AM57X/toolchain/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/bin/../lib/gcc/arm-none-linux-gnueabihf/9.2.1/plugin/include/builtins.h:23:10: fatal error: mpc.h: No such file or directory | #include <mpc.h> | ^~~~~~~ | compilation terminated. | /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/scripts/gcc-plugins/Makefile:47: recipe for target 'scripts/gcc-plugins/arm_ssp_per_task_plugin.so' failed | make[3]: *** [scripts/gcc-plugins/arm_ssp_per_task_plugin.so] Error 1 | /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/scripts/Makefile.build:497: recipe for target 'scripts/gcc-plugins' failed | make[2]: *** [scripts/gcc-plugins] Error 2 | make[2]: *** Waiting for unfinished jobs.... | /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/Makefile:1199: recipe for target 'scripts' failed | make[1]: *** [scripts] Error 2 | /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work-shared/am57xx-evm/kernel-source/Makefile:185: recipe for target '__sub-make' failed | make: *** [__sub-make] Error 2 | ERROR: oe_runmake failed | WARNING: /home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/temp/run.do_compile.3704:1 exit 1 from 'exit 1' | ERROR: Execution of '/home/stranzjm/Yocto/build/ti-processor-sdk-linux-08_02_01_00/arago-tmp-external-arm-glibc/work/am57xx_evm-linux-gnueabi/linux-ti-staging/5.10.100+gitAUTOINC+7a7a3af903-r7b.arago5_psdkla_14/temp/run.do_compile.3704' failed with exit code 1 ERROR: Task (/home/stranzjm/Projekte/ti-am57x/PROCESSOR-SDK-LINUX-AM57X/ti-processor-sdk-linux-08_02_01_00/yocto-build/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_5.10.bb:do_compile) failed with exit code '1' NOTE: Tasks Summary: Attempted 1527 tasks of which 1525 didn't need to be rerun and 1 failed. NOTE: Writing buildhistory NOTE: Writing buildhistory took: 1 seconds