Hii Ti Support Team,
I am using AM3359 Based processor and i have generated u-boot-spl.bin and u-boot.img from u-boot SDK but When I loaded both images I got data abort error as shown below:
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC
U-Boot SPL 2019.01-g1ebdbc7-dirty (Jan 24 2023 - 13:33:31)
Load U-Boot image...
CxyzModem - CRC mode, 3(SOH)/371(STX)/0(CAN) packets, 4 retries
Loaded 379352 bytes
U-Boot SPL 2019.01-g1ebdbc7-dirty(Jan 24 2023 - 13:33:31)
I2C: ready
DRAM: 256 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<8f761270>] lr : [<8f760d9c>]
sp : 8f32fe58 ip : 00000062 fp : 8f334be8
r10: 8f3327c8 r9 : 8f32ff38 r8 : 8f3327d0
r7 : 8f32fed4 r6 : 000000d6 r5 : 8f334bec r4 : 8f330008
r3 : 00000000 r2 : 00000001 r1 : 00000001 r0 : 00000000
Flags: NzCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
Pleaser Help us on this
Thanks and Regards
Rakshith