Part Number: TMS320VC33
I have an emulator which supports only ccs4 or ccs3. How can I find out a copy of ccs3? Can anyone kindly give me a copy? I understand CCS3 is removed from the download list. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320VC33
I have an emulator which supports only ccs4 or ccs3. How can I find out a copy of ccs3? Can anyone kindly give me a copy? I understand CCS3 is removed from the download list. Thanks.
Hello Andrew,
Which device are you working with? If you are working with TMS320VC33, note that CCS3 does NOT support that device.
I see you have another related thread:
Let's continue discussion there.
Thanks
ki
As I know, CCS3 needs an add-on patch to support VC33.
This is false. There is no way to add VC33 support to CCS 3.3.
As far as you, does CCS4 support TMS320VC33 with any software patches?
No. No version of CCS ever supported VC33. You need CC (without the "S"). CC4 supported VC33.
Thanks
ki
No. No version of CCS ever supported VC33. You need CC (without the "S"). CC4 supported VC33.
Same information here: