Other Parts Discussed in Thread: OMAP-L138
Dear E2E:
Thank you for your help.
I have a question about Emulation Debug Boot.
In the document "Using the OMAP-L138 Bootloader" (SPRAB41C) Appendix A "Emulation debug" and Section 3.3 "Emulation Debug Boot" describes the emulator connection to OMAP-L138.
It looks like the "boot bits" must be set to 0001 1110 before the Emulator is connected to JTAG.
Is this true?
We plan to boot from NOR FLASH in normal operation.
We don't plan to have any switches on PCB.
We can add some logic which is activated when the Emulator is plugged in.
Will this work?
We have boot bits set to NOR FLASH but when we connect the emulator - the boot mode switches to Emulator Debug mode.
Will it be OK?
This is a little surprising feature - we need to change the HW before connecting to JTAG interface.
Usually the processors do not require that.
Thank you for your help,
Boris Ruvinsky