Other Parts Discussed in Thread: ADS8556
Hi,
I have 2 ADC (ADS8556) outputs connected to 2 serializers of the McASP in C6713.
The ADC is a 6-channel device. Once the conversion starts, it sends the 6 channel data-words
on its output (SDO_A). I want to receive 12-channel data from both the ADC's.
Want to use the DAT port for receiving. If I enable only one ADC or one serializer, I am able to get
all the 6-channels.
I have a question : if I enable the other serializer for the other ADC, can I read 12 words from the DAT port cconsecutively?
Because, the FS to both the ADC's is same and the CONVST_x signals to both the ADCs are also same.
Aditi.