This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5729: How we can debug c code using code composer studio for beaglebone-ai in linux

Part Number: AM5729


Hi,

I installed  Processor SDk  Linux Version 06.03.00.016 and beaglebone-ai with SD card .so, how can I debug  c code using ccs 9 .3

Do i want debug the code using c type USB which generate power supply to the board ?

To verify connection which type of emulator should i select in ccs ? (XDS100)

What part number should i want to mention  for Target configuration ? 

Do i want to debug with only ccs or there is any other way ?

Regards ,

Mounika