This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: SK-AM62 DDR size configuration

Part Number: SK-AM62
Other Parts Discussed in Thread: SYSCONFIG

Currently SK-AM62X EVM board DDR with 2GB size in bootloader is setting as below

arch/arm/dts/k3-am62x-r5-sk-ms5t04-common.dtsi

        memory@80000000 {

                device_type = "memory";

                /* 2G RAM */

                reg = <0x00000000 0x80000000 0x00000000 0x80000000>;

 

        };

arch/arm/dts/k3-am62x-sk-common-ms5t04.dtsi

        memory@80000000 {

                device_type = "memory";

                /* 2G RAM */

                reg = <0x00000000 0x80000000 0x00000000 0x80000000>;

 

        };

How to configuration DDR size with 4GB?

  • Hello,
    Have you tried the following changes in the *.dts
    - reg = <0x00000000 0x80000000 0x00000000 0x80000000>; // 2G DDR
    + reg = <0x00000000 0x80000000 0x00000001 0x00000000>; // 4G DDR

    Here is an early e2e post on DDR configuration in AM64x R5-SPL for your reference.
    e2e.ti.com/.../3852740
    Best,
    -Hong

  • Thanks Hong, but still have a question, my Micron 4GB DDR model is MT40A2G16TBB-062E. Does this configuration you provided fit MT40A2G16TBB-062E model?

  • Hello,
    Some good reference on DDR configurations:
    [1] AM62x DDR Board Design and Layout Guidelines
    www.ti.com/.../sprad06
    [2] From [1], To facilitate software configuration of the DDRSS, use the DDR Subsystem Configuration Tool in SysConfig (https://dev.ti.com/sysconfig)
    Here is a useful link in MCU+SDK on how to use SysConfig tool for DDR configurations.
    software-dl.ti.com/.../DRIVERS_DDR_PAGE.html
    As noted in the README file from SysConfig on DDR (in attachment), it supports AM64x\AM62x\AM243x\AM62Ax, and can be used with SDKs (Linux/u-boot, MCU+SDK SBL)...

    Best,
    -Hong

    # AM64x\AM62x\AM243x\AM62Ax DDR Register Configuration (v9.05)
    
    ## Procedure:
    1) Select Add button at the top and choose the DDR Memory Type.  Fields will be populated with default values for AM64x\AM62x\AM243x\AM62Ax EVMs<br>
    2) Modify parameters based on your DDR device. Hover mouse pointer over each parameter and choose the help icon (?) for more explanation<br>
    3) The 'Generated Files' section on the right has output files for your software (uboot, RTOS, or GEL) that can be saved.  A SysConfig configuration script can also be saved and then reloaded at a later time using File->Open in Sysconfg.
    
    ### GEL
    The resulting .gel file should be placed in the CCS installation for your device, for example ccs\ccs_base\emulation\gel\AM64x\AM64_DDRSS, and loaded using a GEL_LoadGEL instruction (see example in ccs\ccs_base\emulation\gel\AM64x\AM64_DDRSS\AM64x_GP_EVM.gel)
    
    ### CMM
    The resulting .cmm file should be placed in the Lautherbach installation for your device.
    
    ### Linux u-boot
    The resulting .dtsi file should be placed in arch/arm/dts, and the include statement in k3-am642-r5-<board>.dts (eg., k3-am642-r5-evm.dts for the GP EVM, or k3-am642-r5-sk.dts for the StarterKit) should reference the new .dtsi file.  The DDR driver will properly set the DDR frequency and initialize the DDR controller using the information in this .dtsi file
    
    ### MCU+ SDK (RTOS)
    The resulting .h file should be placed in mcu_plus_sdk_<device>_<version>\source\drivers\ddr\v0\soc\am64x_am243x  
    and included by using the SysConfig for SDK tool when building your code.  Please refer to the SDK API Guide mcu_plus_sdk_<device>_<version>\docs\api_guide_am64x\DRIVERS_DDR_PAGE.html for more information
    
    ## Revision History
    v8.10: initial stable version.  Changes from previous versions include:
    - added read/write DBI selection for LPDDR4/DDR4.  Default to enable write DBI for LPDDR4, read DBI for DDR4 to improve power supply noise and improve overall signal integrity
    - changed default value of CA ODT to 60ohm for both LPDDR4 and DDR4
    - updated RTOS output to fix #ifdef
    - periodic write DQ leveling disabled to improve realtime performance
    - disabled "always-on" mode of the input enables for data bytes for power optimization
    - disabled VREF controller for addr/cmd signals for power optimization<br>
      
    v8.40: provides improved operation at 1600MTs for both LPDDR4 and DDR4.  Changes from previous version include:
    - changed default value CTRLUPD_AREF_HP_ENABLE=0
    - changed default value LPI_WAKEUP_EN=0
    - changed cal_clk divider and PVT calibration interval.  This change provides significant stability improvements for LPDDR4 and DDR4 operation at 1600MTs
    - fixed TOSCO_F0 calculation for LPDDR4
      
    v8.80: added support for AM62x release, added support for high temp operation, Other misc fixes to align with documentation: 
    - CTL_165[11]=1 (LPI_WAKEUP_EN) only applicable for AM62x
    - CTL_321[23:8] = 0xFFFF (CS_MSK_1) corrected value when rank 1 disabled
    
    v9.04: 
    -changed wrlvl_delay_early_threshold=0x100 to allow write leveling to complete successfully for wider array of layouts<br> 
    -add cmm output<br>
    -LPDDR4: phy_rddqs_latency_adjust changed to 0 default recommendation (this value gets optimized during training)<br> 
    -LPDDR4: optimized training loops to support 1 operating frequency<br>
    -LPDDR4/DDR4: optimized IO calibration configuration based on operating frequency<br>
    -LPDDR4/DDR4: optimized internal calibration clock based on operating frequency<br>
    -LPDDR4: changed default MR22 ODTE-CS=1<br>
    -LPDDR4: changed rx_ctle_cs default to No Boost<br>
    -AM62x dual rank support<br>
    -updated to use sysconfig v1.15<br>
    -public release for AM62A LPDDR4 support<br>
    v9.05:
    -cleaned up supported frequencies
    
    
    

  • This one is the TI EVM Micron 2G used:à 3200MT/s, 2933MT/s Micron 2G : 8 internal banks (x16): 2 groups of 4 banks each

    This one is their PCB mounted Micron 4G à 3200MT/s, Micron 4G : 128 Meg x 16 x 16 banks x 1 rank

     

    This 4G DDR is actually have 16Gbx2 (16 banks) in the single die, which only can be run on the 3200MT/s.

    The TI EVM is using 8 banks.

     

    What’s the correct DDR setting for this Micron 4G DDR? Can you give us some comments?

    Should we modify the R5 codes for making it work as well?

  • Hello,
    I'm looping in my colleague on his comments on this specific DDR support on AM62x.
    Best,
    -Hong

  • Rio, please check https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1191664/am625-ddr4-dual-die-support

    this has guidance on how to support the 4GByte, dual die DDR4 device

    Regards,

    James

  • Hello,
    As the e2e referenced by James, the DDR DT node needs to be adjusted as below after completing DDR parameters setup using SysConfig tool
    for your specific DDR.

    The 1st 2GB: 0x000000000 80000000 to 0x00000000 FFFFFFFF
    The 2nd 2GB: 0x000000008 80000000 to 0x00000008 FFFFFFFF
    
     	memory@80000000 {
     		device_type = "memory";
    -		/* 2G RAM */
    -		reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    +		/* 4G RAM */
    +		reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
    +		      <0x00000008 0x80000000 0x00000000 0x80000000>;
     	};

    Best,
    -Hong