Part Number: AM625
Can you confirm that the EXTINTn signal is routed to the GIC500 as SPI 256?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ISEE,
Thank you for the query.
Please refer below:
Yes it does. There is a hop in the path from the extint_n signal to the GIC where the signal is inverted.
Additional info:
glue_ext_intn is an inversion of the ext_intn pin. ext_intn is positive low. Before this signal is routed to the interrupt destination, it is made positive high going through this glue logic. Ext_intn is used as nmi interrupt source from external input through the pin.
Regards,
Sreenivasa