Part Number: TDA4VM
Hi experts.
I am using custom board based on TDA4VM.
About SER/DES , my board have following connections.
Flow "Camera -> UB953 -> UB954 -> Processor" is already working.
Currently , my board have additional SER(UB953).(red circled)
I confirmed that I have access to the SER via I2C.
I want to bypass the input camera image from UB954 to the SER.(green arow)
Question: It is possible? What changes are needed?
SDK version:
ti-processor-sdk-rtos-j721e-evm-08_00_00_12
ti-processor-sdk-linux-j7-evm-08_00_00_08