This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: How to create new mac address using DSA?

Part Number: AM3352

Hi,

EVM-SK is what I am using and the 2 physical Ethernet port is configured to switch mode.

You can see the mac address of eth0 is "90:59:af:6e:02:43" as below and it's the interface mac address.

The requirement what I ask is another mac address for Por1 and Port2 respectively.

The mac address should be "90:59:af:6e:02:44" for Port1 and "90:59:af:6e:02:45" for Port2.

Do you know how to apply it using DSA? Thanks.

eth0      Link encap:Ethernet  HWaddr 90:59:af:6e:02:43
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

SDK: ti-processor-sdk-linux-rt-am335x-evm-08.02.00.24

Hardware : TI AM335x EVM-SK