This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721S2: TDA4Eco

Part Number: PROCESSOR-SDK-J721S2

Hi team,

Here's an issue from the customer may need your help:

SDK: ti-processor-sdk-rtos-j721s2-evm-08_05_00_11

The SBL program under PDK by default supports the flash chip S28HS512T. Does the MT35XU512ABA1G12 flash support?

The ospiFlash model on the customer board is MT35XU512ABA1G12, and after changing the corresponding ID to MT35XU512ABA1G12, Board_flashOpen failed is displayed in the log. However, after uboot is started with SD card, ospiFlash can be read and written in uboot.

So could you please help confirm if this version of SDK supports MT35XU512ABA1G12? If so, what software modifications are required? Thanks.

Best Regards,

Cherry