This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM62A7: Import SDK Examples: Solving the AM62Ax Recognition Issue in CCS

Part Number: AM62A7

Hi,

While trying to import SDK example into CCS 12.1.0, some might encounter the problem stating "AM62Ax device not recognized".

A more detailed overview of the issue can be seen in the screenshot below.

Lets look at a quick fix for the same which will hardly take less than five minutes of your time.

Regards,

Vaibhav

  • Text Solution:

    • You will need patch files which will be added to the CCS, more specifically the CCS version 12.1.
    • Patch Files:3365.AM62AxCSP.zip
    • Simply go ahead and extract the patch file into your CCS directory and you are halfway done.
    • Now you can easily recognize the AM62A device while setting up the target configuration.
    • At this point, you might still face issue while importing examples, so simply go ahead and reinstall CCS and this will hardly take not more than two minutes.
    • Restart CCS and now you should be able to import the examples.

    Video Explanation:

    8446.am62a device recognize.mp4

    Guide to setting up Target Configuration: Custom Target Configurations

    Thanks