I am able to configure davicom 9601 on the host usb 1.1 port. I have also configured the kernel to support the Ethernet gadget on the usb 2.0 OTG port.
somehow when try to support both of them in the same configuration the host 1.1 is not recognizing the usb Ethernet dongle.
is there a way to configure the kernel to support both at the same time ?
I am using kernel 2.6.33-rc4 from psp 3.20.0.0.14
Thanks.
Roy