Part Number: TDA4VM
Hi, ti experts,
We have the following problems with tda4vm sdk8.2 (Linux sdk & rtos sdk), please help to confirm:
1. Does the tda4vm frequency decrease when the cpu temperature is too high? At what temperature does the frequency drop?
2. Is the frequency of each core going to be reduced? For example, A72, MCU1-0, MCU12-0, MCU3-0, and so on.
3. Will reducing the frequency cause the system to stall? (Linux & rtos)?