This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Available CSI2 RX bandwidth

Part Number: AM623


Hello,

Let me confirm about below.

* According to feature of following datasheet, CSI2 can accept up to 2.5Gbps.(This means up to FHD(1920x1080@60 with YUV16) can be accepted.)

- Support for 1,2,3 or 4 data lane mode up to 2.5Gbps.
(I understand that 625Mbps can be accepted per lane.)

However, on the other hand, there is following description in "7.11.5.3 CSI-2"

- Support for 1,2,3 or 4 data lane mode up to 1.5Gbps.
(I understand that 375Mbps can be accepted per lane.)

It seems that bandwidth which CSI-RX can accept shrink.
Could you please tell me which information is correct ? 

BR,