Other Parts Discussed in Thread: SYSBIOS
Hi,
I post again the same message I have posted on june 22th.
Hi,
I have some questions related to DAT_open and DAT_copy functions.
1.- Is possible to use with the c6678?
2.- How the DAT_copy function takes advantage of the 10 transfer controllers existents in the C6678?
3.- Is possible to use the DAT_copy function and the CSL EDMA3 functions together?
4.- How DAT_copy affects the performance of the EDMA due that it adds another API layer?
5.- DAT_open and DAT_copy functions need to work only with the sysBIOS or also they can be used without os?
6.- Where is possible to find an example for c6678 that uses DAT_open and DAT_copy under sysBIOS that works. I took the code found in the three folders under: C:\Program Files\Texas Instruments\edma3_lld_02_11_01_02\examples\CSL2_DAT_DEMO\src\ in a new sysBIOS project but I didn't succeed to build the example.
Thanks in advance.
Shmulik.